Toradex®: Asymmetric Heterogeneous Architecture for Real-Time and Low-Power Performance

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Toradex®: Asymmetric Heterogeneous Architecture for Real-Time and Low-Power Performance

Toradex®: Asymmetric Heterogeneous Architecture for Real-Time and Low-Power Performance

The talk will first outline the trade-off between heterogeneous architectures and more traditional approaches of using external controllers. Asymmetric Heterogeneous Architectures are found in NXPs i.MX 6SoloX, i.MX 7 and i.MX 8 SoCs. The discussion is centered around the balancing robot and an IoT use case, including live demos. In the second part of the talk, we’ll discuss the software challenges of such an architecture. We’ll focus on using the Linux frameworks remoteproc & rpmsg which are the de-facto standard frameworks used to support such architectures in various. Finally, we’ll look at the robot’s and IoT Demo Qt-based graphical application that interfaces with rpmsg to communicate with the FreeRTOS firmware.

添付
評価なし
バージョン履歴
最終更新日:
‎06-18-2018 06:11 PM
更新者: