Applications for High-Performance Layerscape Processors (LX2160A)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Applications for High-Performance Layerscape Processors (LX2160A)

Applications for High-Performance Layerscape Processors (LX2160A)

LX2160A is NXP’s highest performance multicore device with 16 Arm-v8 64-bit A72 cores at up to 2.2 GHz. It also has 24 SerDes lanes running at 25 GHz supporting dual 100GE interfaces and up to 24 lanes of PCIe Express. It has security acceleration to 50 Gbps and data compression/decompression to 100 Gbps. This session will explain LX2160A’s suitability for the main target applications (5G, industrial, ADAS, storage, NIC, and edge routing), benchmarking results (CoreMark, Dhrystone, DPDK, SpecInt, …), software and reference board enablement, 3rd-party board solutions, and how it stacks up against the Xeon-D family of devices.

Tags (1)
Attachments
No ratings
Version history
Last update:
‎09-09-2019 06:56 AM
Updated by: