Taplinx iOS - how to select application 0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Taplinx iOS - how to select application 0

503 次查看
DamianD
Contributor III

When using taplinx ios library i do following code:

 

 

TLLibraryManager.Shared.DESFireEV3Instance.SelectApplicationWithAppID(0, (success) =>
{    
    if (success == false)
    {        
        return;
    }
    TLLibraryManager.Shared.DESFireEV3Instance.GetApplicationIDsOnCompletion((bool success) =>
    {
        
    });

 

 

With added logging in apduHandler i see what gets sent and returns from card. So for selection app with id 0 following bytes are sent: 5A000000 and returned 00 (which is correct), so in callback to selecting app i get success - however after that when i send  api to get all application ids, nothing gets sent to card (no apdu command) and in device log i get following entries:

 

 

Time	Device Name	Type	PID	Tag	Message
Nov  7 22:58:16	iPhone	Notice	5584	MobileFacilityApp	Caught an exception (
Nov  7 22:58:16	iPhone	Notice	5584	MobileFacilityApp	Exception Caught: com.nxp.nfclib.exceptions.UsageException: Application 0 must be selected when using getApplicationIDs()

 

 

1. Why is library not remembering that app with id 0 was already selected?

2. how to actually get that list of ids? declaration of that method:

- (void)getApplicationIDsOnCompletion:(completionBlockWithResult)completion;

states that it only returns BOOL determinig of action was success or not - how do i get back the actual list of applications?

标签 (1)
0 项奖励
回复
0 回复数