Implementing Mifare SDK in React Native

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Implementing Mifare SDK in React Native

1,700 Views
Japhetism
Contributor I

I'm encountering some problems with integrating the Mifare SDK into my React Native project. Could anyone assist me with this?

Labels (3)
0 Kudos
Reply
2 Replies

1,538 Views
react-masters
Contributor I

Integrating the Mifare SDK into a React Native project can sometimes be tricky, especially when dealing with native modules and dependencies. I recommend the following steps to help you troubleshoot and potentially resolve the issue:

  1. Check Compatibility: Ensure that the version of the Mifare SDK you're using is compatible with your React Native version. Sometimes, mismatches between SDK versions and React Native versions can cause problems.

  2. Linking Native Modules: If the SDK has native dependencies, properly link those native modules. In newer React Native versions, auto-linking should handle this automatically, but for older versions, you may need to run react-native link or manually update the Android and iOS native files.

  3. Permissions: NFC technology requires specific device permissions. Ensure that you've added the correct permissions in your AndroidManifest.xml for Android or in Info.plist for iOS.

  4. Check Documentation: Refer to the official Mifare SDK documentation for any specific instructions related to integrating with React Native. Additional steps might be required to correct initialization.

  5. Error Logs: Share the exact error or issue you're encountering (logs, screenshots, etc.), as that could provide more context to those assisting you.

If you still need further help, feel free to share your setup or error details, and we can dive deeper into resolving this.

React Masters is a professional React training institute that teaches the fundamentals of React in a way that can be applied to any web project
0 Kudos
Reply

1,640 Views
ukcas
NXP Employee
NXP Employee

Hello Japhetism,

Sorry, at the moment we do not support integrating TapLinx library into third party frameworks like React Native. Anyway, as per React Native presentation, integrating shall be possible.

Best regards.

0 Kudos
Reply