why usdpaa sra application can not run T2080

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

why usdpaa sra application can not run T2080

1,399 Views
liujianbo
Contributor II

Hi Experts:

About the USDPAA SRA application, in SDK's doc, it state:

/**********************************************************************/

Currently, it can run on P3041DS/P4080DS/P5020DS/T4240QDS/B4860QDS board.

/**********************************************************************/

T4080 and T2080 have the the same e6500 core, and the similiar arch(except the number of interface), why T2080 can not run this application, is this a doc issue or there is do some reason?

Thanks a lot for your time!!

Labels (1)
Tags (4)
1 Reply

1,168 Views
tapyang
Contributor III

Hi,I have the same question!I want to know the reason too.