why usdpaa sra application can not run T2080

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

why usdpaa sra application can not run T2080

1,393件の閲覧回数
liujianbo
Contributor II

Hi Experts:

About the USDPAA SRA application, in SDK's doc, it state:

/**********************************************************************/

Currently, it can run on P3041DS/P4080DS/P5020DS/T4240QDS/B4860QDS board.

/**********************************************************************/

T4080 and T2080 have the the same e6500 core, and the similiar arch(except the number of interface), why T2080 can not run this application, is this a doc issue or there is do some reason?

Thanks a lot for your time!!

ラベル(1)
タグ(4)
1 返信

1,162件の閲覧回数
tapyang
Contributor III

Hi,I have the same question!I want to know the reason too.