vxworks bootrom bank

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

vxworks bootrom bank

Jump to solution
1,435 Views
pritokhatri
Contributor I

Hi All,

Can anyone tell which switch needs to be changed in t2080rdb board for choosing the vxworks bootrom bank????

Labels (1)
0 Kudos
1 Solution
1,189 Views
bpe
NXP Employee
NXP Employee

NOR Flash bank addresses are changed by SW3[5:7] DIP switch. These settings affect the boot process only if NOR is selected to be

the boot ROM by SW3[4]. See T2080RDBUG Table 2-9 and notes below it.

Note, no VxWorks images are pre-programmed to any T2080RDB Flash/bank. Consult at Wind River for correct

image preparation, programming and booting.


Have a great day,
Platon
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
1,190 Views
bpe
NXP Employee
NXP Employee

NOR Flash bank addresses are changed by SW3[5:7] DIP switch. These settings affect the boot process only if NOR is selected to be

the boot ROM by SW3[4]. See T2080RDBUG Table 2-9 and notes below it.

Note, no VxWorks images are pre-programmed to any T2080RDB Flash/bank. Consult at Wind River for correct

image preparation, programming and booting.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos