vxworks booting for t2080rdb board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

vxworks booting for t2080rdb board

1,049 Views
pritokhatri
Contributor I

Hi All,

I am trying to boot vxworks using uboot for t2080rdb board.

I tried to download the image over tftp but after giving bootvx command it comes and hangs at asshown

Filename 'vxWorks'.

Load address: 0x1000000

Loading: #################################################################

         ##########################

         4.5 MiB/s

done

Bytes transferred = 1328040 (1443a8 hex)

=> bootvx 1000000

## Ethernet MAC address not copied to NV RAM

## Using bootline (@ 0x4200): root=/dev/ram rw console=ttyS0,115200

## Starting vxWorks at 0x00100000 ...

Labels (1)
0 Kudos
Reply
0 Replies