t4240 ddr validation target connections fail

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

t4240 ddr validation target connections fail

ソリューションへジャンプ
2,927件の閲覧回数
muaxi8
Contributor V

t4240 custom board. 

Now my board is stuck in the DDR initialization section, so I  created a DDR project using

CodeWarrior, but CodeWarrior cannot connect to the DDR. 

CodeWarrior Debug can connect, DDR verification is not,why? 

Can you check my CW configuration for me

muaxi8_0-1659606684969.png

I want to know if my connection configuration is correct ?

muaxi8_0-1659606296071.png

 

 

0 件の賞賛
返信
1 解決策
2,861件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

It seems that you didn't open the correct CCS console.

Please close CodeWarrior IDE and all CCS consoles.

Then open CodeWarrior IDE again, click Target Connection, the CCS console will be popped up automatically, please use this CCS console, type "log v" and connect to the target board again, the low level CCS log will be printed out.

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
2,901件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

When you click "Start Validation" the CCS(CodeWarrior Connection Sever) will be popped up at the right bottom of the Window task bar, please open CCS console, type "log v" then click "Start Validation" again, the low level CCS log will be printed in CCS console, please capture this CCS log to me to do more investigation.

0 件の賞賛
返信
2,899件の閲覧回数
muaxi8
Contributor V

 

My current problem is that the "Start Validation" is grayed out and I can't click on it

muaxi8_0-1660041846027.png

 

0 件の賞賛
返信
2,888件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

You use T4240 processor, why did you configure the "System" as T2080?

If your problem remains, please capture the CCS log to me to do more investigation.

 

0 件の賞賛
返信
2,886件の閲覧回数
muaxi8
Contributor V

I have two boards, a T2080RDB and a T4240 custom board.

t4240 custom boadr is discrete ddr.

No output is generated after the target connection.

muaxi8_0-1660207029869.png

 

muaxi8_1-1660207054995.png

 

this is my  codewarrior.  I don't know because something is wrong with the configuration ?

muaxi8_1-1660209871900.png

 

 

0 件の賞賛
返信
2,862件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

It seems that you didn't open the correct CCS console.

Please close CodeWarrior IDE and all CCS consoles.

Then open CodeWarrior IDE again, click Target Connection, the CCS console will be popped up automatically, please use this CCS console, type "log v" and connect to the target board again, the low level CCS log will be printed out.

0 件の賞賛
返信