Hello. I am using a version of build_t4240rdb-64b But with the following additional options in the file pointed to by KERNEL_DEFCONFIG
CONFIG_NET_IP_TUNNEL=y
CONFIG_INET_XFRM_TUNNEL=y
CONFIG_INET_TUNNEL=y
CONFIG_INET_XFRM_MODE_TUNNEL=y
CONFIG_INET6_XFRM_MODE_TUNNEL=y
CONFIG_TUN=y
CONFIG_NETFILTER_NETLINK=y
CONFIG_NETFILTER_NETLINK_QUEUE=y
CONFIG_NETFILTER_NETLINK_LOG=y
CONFIG_NF_CT_NETLINK=y
CONFIG_SCSI_NETLINK=y
CONFIG_IP_ADVANCED_ROUTER=y
CONFIG_NET_SCH_INGRESS=y
CONFIG_NET_SCHED=y
CONFIG_IP_MULTIPLE_TABLES=y
CONFIG_NETFILTER_XT_TARGET_MARK=y
After bringing up the image I am now trying to add a bridge device, but I get -
root@t4240rdb:~# ip link add name br0 type bridge
RTNETLINK answers: Operation not supported
Please let me know what configuration option I am missing.
Thanks a lot,
Elliot
解決済! 解決策の投稿を見る。
Hello Elliot Black,
Please Enable Ethernet bridging in linux kernel as the following.
[*] Networking support --->
Networking options --->
<*> 802.1d Ethernet Bridging
[*] IGMP/MLD snooping (NEW)
Please refer to the following Kernel options.
root@t2080rdb:~# zcat /proc/config.gz | grep BRIDGE
CONFIG_BRIDGE_NETFILTER=m
# CONFIG_BRIDGE_NF_EBTABLES is not set
CONFIG_BRIDGE=y
CONFIG_BRIDGE_IGMP_SNOOPING=y
In addition, you also could refer to the following commands to setup bridge.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hello Elliot Black,
Please Enable Ethernet bridging in linux kernel as the following.
[*] Networking support --->
Networking options --->
<*> 802.1d Ethernet Bridging
[*] IGMP/MLD snooping (NEW)
Please refer to the following Kernel options.
root@t2080rdb:~# zcat /proc/config.gz | grep BRIDGE
CONFIG_BRIDGE_NETFILTER=m
# CONFIG_BRIDGE_NF_EBTABLES is not set
CONFIG_BRIDGE=y
CONFIG_BRIDGE_IGMP_SNOOPING=y
In addition, you also could refer to the following commands to setup bridge.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
After adding the following configuration options to my CONFIG file I recompiled the kernel and the linux image with the following commands -
bitbake -c cleansstate virtual/kernel
bitbake -f virtual/kernel -c compile
bitbake virtual/kernel
bitbake fsl-image-full
and I am able boot the image and create a bridge device with the following command -
brctl addbr br0.
Thank you.