powerpc64-fsl-linux-ld.bfd: cannot find -lgcc

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

powerpc64-fsl-linux-ld.bfd: cannot find -lgcc

1,989件の閲覧回数
muaxi8
Contributor V

for t4240rdb-64b:

I downloaded the U-boot from 《QorIQ SDK 2.0 Documentation For QorIQ Processors》and set the environment variables :. /opt/fsl-qoriq/2.0/environment-setup-ppc64e6500-fsl-linux 

it can't find libgcc.a  when I make uboot.

powerpc64-fsl-linux-ld.bfd: skipping incompatible /opt/fsl-qoriq/2.0/sysroots/ppc64e6500-fsl-linux/usr/lib64/powerpc64-fsl-linux/4.9.2/libgcc.a when searching for -lgcc
powerpc64-fsl-linux-ld.bfd: cannot find -lgcc
powerpc64-fsl-linux-ld.bfd: skipping incompatible /opt/fsl-qoriq/2.0/sysroots/ppc64e6500-fsl-linux/usr/lib64/powerpc64-fsl-linux/4.9.2/libgcc.a when searching for -lgcc
powerpc64-fsl-linux-ld.bfdmake[2]: *** [examples/standalone/hello_world] Error 1: cannot find
-lgcc
make[2]: *** Waiting for unfinished jobs....
make[2]: *** [examples/standalone/sched] Error 1
make[1]: *** [examples/standalone] Error 2
make: *** [examples] Error 2

muchx@ubuntu:~/work/t4080/QorIQ-SDK-V2.0-20160527-yocto/build_t4240rdb-64b/tmp/work/t4240rdb_64b-fsl-linux/u-boot-qoriq/2016.01+fslgit-r0/git$

0 件の賞賛
返信
2 返答(返信)

1,969件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please install E6500 32 bit Toolchain.

$ source /opt/fsl-qoriq/2.0/environment-setup-ppce6500-fsl-linux

$ make T4240RDB_defconfig

$ make -j 4 ARCH=powerpc CROSS_COMPILE=powerpc-fsl-linux-

0 件の賞賛
返信

1,955件の閲覧回数
muaxi8
Contributor V

32 bit T4240rdb compile will get stuck at 99 percent.

muaxi8_0-1649214944077.png

 

0 件の賞賛
返信