lauterbach tool license support for T1024RDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lauterbach tool license support for T1024RDB

Jump to solution
1,671 Views
veerendranathj
Contributor III

Hi,

We are planning to buy T1024RDB board. Do we have to buy lauterbach (Trace32, JTAG) tool license for T1024 separately or we will get it with T1024RDB board?

We already have lauterbach  (Trace32, JTAG) license, cables and devices for P2041RDB. If we need to buy extra license... How can we update existing setup for T1024RDB.

Thanks and Regards,

Veerendranath

Labels (1)
0 Kudos
Reply
1 Solution
1,456 Views
alexander_yakov
NXP Employee
NXP Employee

As far as I know, the list of supported devices is stored in Lauterbach debug probe tip, and therefore depends on tip you are using.

To check if the device is supported please run Trace32, select "CPU" in menu and than again press "CPU" button in the window.

No, Lauterbach license is not included in T1024RDB package.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,457 Views
alexander_yakov
NXP Employee
NXP Employee

As far as I know, the list of supported devices is stored in Lauterbach debug probe tip, and therefore depends on tip you are using.

To check if the device is supported please run Trace32, select "CPU" in menu and than again press "CPU" button in the window.

No, Lauterbach license is not included in T1024RDB package.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply