Hi,
I have QorIQ-sdk-V2.0-20160527-yocto and I can build Image for t1042d4rdb machine
I want to get cpu temperature and monitor it in my application, but I cant find the temperature in its linux!
I have QorIQ-sdk document too, in it said that I must check this parameter in kernel :
<*> CPU frequency scaling driver for NXP QorIQ SoCs
but I couldnt find it ! there is :
<*> CPU frequency scaling driver for Freescale QorIQ SoCs
in menuconfig.
there is a Device Tree Binding section in document too, what I must do with IT ?
Im new in Embedded Linux developing, can you help me to how I can access to cpu temperature ??
I want a simple road map to do
sorry for poor English.
thank you!
I add these variables to kenel config :
CONFIG_QORIQ_CPUFREQ=y
CONFIG_THERMAL=y
CONFIG_CPU_THERMAL=y
CONFIG_QORIQ_THERMAL=y
after building and booting the board, I see these log in kernel boot log :
qoriq_thermal ffe0f0000.tmu: Failed to register thermal zone device -517
qoriq_thermal ffe0f0000.tmu: Failed to register thermal zone device -517
qoriq_thermal ffe0f0000.tmu: Failed to register thermal zone device -517
and there is no "/sys/class/thermal/thermal_zone0/" directory in /sys/class/thermal/
how I can get Cpu temperature ??
can you help me? Is there any way to get cpu temperature
Use the option "Freescale QorIQ SoCs".
thanks a lot !
and what about device Tree code that mentioned in document??
selecting neccesary option in kernel is enough for my purpose ??
thanks, you are right
but my question now is about cpu temperature, because All of development are done on this version and now I want only cpu temperature
then I can update and cotinue...
You wrote:
> I have QorIQ-sdk-V2.0-20160527-yocto
Please install update "QorIQ Linux SDK v2.0-1703" available for download here:
Hi,
for using this article it is necessary to use SCFW Porting Kit
Please also check processor revision, as old may not work with the latest Linux
releases described on i.MX Software and Development Tools | NXP paymydoctor
Best regards.