I want to generate cryptodev.ko standalone and not with kernel,
so i tried following from sdk document page number --> 1260 (QorIQ SDK v2.0=1703 doc)
• Build cryptodev
$ cd <sdk-dir>/sources/cryptodev
$ make
$ sudo make modules_install
$ sudo install -D crypto/cryptodev.h /usr/include/crypto/cryptodev.h
But there is no makefile at the above place
How to do it for t2080
已解决! 转到解答。
Hello sameerarvikar,
I assume that you have installed SDK 2.0 Toolchain in /opt/fsl-qoriq/2.0/.
$ source /opt/fsl-qoriq/2.0/environment-setup-ppce6500-fsl-linux
$ unset LDFLAGS
$ make -C /home/b25805/QorIQ-SDK-V2.0-20160527-yocto/build_t2080rdb/tmp/work/t2080rdb-fsl-linux/linux-qoriq/4.1-r0/build/ M=/home/b25805/QorIQ-SDK-V2.0-20160527-yocto/build_t2080rdb/tmp/work/t2080rdb-fsl-linux/cryptodev-qoriq-module/1.8-r0/cryptodev-linux-1.8 ARCH=powerpc CROSS_COMPILE=powerpc-fsl-linux- modules
The build command
$ make -C <Kernel build directory> M=<cryptodev module source> ARCH=powerpc CROSS_COMPILE=powerpc-fsl-linux- modules
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello sameerarvikar,
I assume that you have installed SDK 2.0 Toolchain in /opt/fsl-qoriq/2.0/.
$ source /opt/fsl-qoriq/2.0/environment-setup-ppce6500-fsl-linux
$ unset LDFLAGS
$ make -C /home/b25805/QorIQ-SDK-V2.0-20160527-yocto/build_t2080rdb/tmp/work/t2080rdb-fsl-linux/linux-qoriq/4.1-r0/build/ M=/home/b25805/QorIQ-SDK-V2.0-20160527-yocto/build_t2080rdb/tmp/work/t2080rdb-fsl-linux/cryptodev-qoriq-module/1.8-r0/cryptodev-linux-1.8 ARCH=powerpc CROSS_COMPILE=powerpc-fsl-linux- modules
The build command
$ make -C <Kernel build directory> M=<cryptodev module source> ARCH=powerpc CROSS_COMPILE=powerpc-fsl-linux- modules
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Not able to attach image
Following error is coming :
cryptodev: disagrees about version of symbol crypto_ahash_setkey
cryptodev: Unknown symbol crypto_ahash_setkey (err -22)
like this errors are for follwing symbols
crypto_aead_setauthsize
crypto_alloc_aead
crypto_destroy_tfm
crypto_alloc_ablkcipher
crypto_alloc_ahash
crypto_alloc_base
crypto_ahash_digest
insmod: ERROR: could not insert module cryptodev.ko:invalid parameters
Thanks Yiping,
Its working in t2080RDB
Now i got only kernel-source directory for a custom t2080 board
so it doesn't have a build directory as given in the path in above answer
If i use the cryptodev.ko driver generated for t2080 RDB , i got the errors(please find attachment)
How can i generate it with the kernel-source directory
Regards