compile uboot for t2080qds(ppc)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

compile uboot for t2080qds(ppc)

1,115 Views
gavrielmedina
Contributor I

Hello,

I am really new to linux and trying to learn. I have a T2080QDS evaluation board. I need to build Uboot for ppc.

I have linux, uboot source files, qorIQ linux sdk 2.0.

First i built the qorIQ sdk, now i have: ls opt/fsl-qoriq/2.0/

environment-setup-ppc64e6500-fsl-linux  sysroots environment-setup-ppce6500-fsl-linux    version-ppc64e6500-fsl-linux
site-config-ppc64e6500-fsl-linux       version-ppce6500-fsl-linux          site-config-ppce6500-fsl-linux

Then i do  gavri55@gavri55-PC:~/u-boot$ sudo make T2080QDS_defconfig
  HOSTCC  scripts/basic/fixdep
  HOSTCC  scripts/kconfig/conf.o
  HOSTCC  scripts/kconfig/zconf.tab.o
  HOSTLD  scripts/kconfig/conf
#
# configuration written to .config
#

then gavri55@gavri55-PC:~/u-boot$ sudo make all
scripts/kconfig/conf  --silentoldconfig Kconfig
  CHK     include/config.h
  CFG     u-boot.cfg
/bin/sh: 1: ppc_8xx-gcc: not found
scripts/Makefile.autoconf:79: recipe for target 'u-boot.cfg' failed
make[1]: *** [u-boot.cfg] Error 1
make: *** No rule to make target 'include/config/auto.conf', needed by 'include/config/uboot.release'.  Stop.

i havent defined ARCH or CROSS_COMPILE because i dont know how.

Please help me

Thanks

Labels (1)
0 Kudos
1 Reply

596 Views
Pavel
NXP Employee
NXP Employee

Usually the following commands are used for u-boot building:

bitbake -c cleansstate u-boot

bitbake -c patch u-boot // source of the u-boot

bitbake -c compile -f u-boot

bitbake u-boot

 

See the Section 3.3.13 of SDK 2.0-1703 documentation:

https://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos