change T1042 DDR3

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

change T1042 DDR3

554 次查看
mohsenhaghighat
Contributor III

I want to design a cpu board with T1042 processor that use a 32 bits DDR3 SDRAM.  I do not know anything about its SDK.

because the T1040RDB use a 64bits DDR3 SDRAM and I use a 32 bits, I do not know what problems being in this way.

any body can describe these to problems to me.

thanks

标签 (1)
0 项奖励
1 回复

370 次查看
ufedor
NXP Employee
NXP Employee

No additional precautions have to be done if SPD EEPROM (address 0x51 connected to the I2C1) with correct data is present.

Please refer to the following U-Boot source files:

/include/configs/T104xRDB.h

/drivers/ddr/fsl/ddr3_dimm_params.c

/drivers/ddr/fsl/main.c

0 项奖励