change T1042 DDR3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

change T1042 DDR3

556件の閲覧回数
mohsenhaghighat
Contributor III

I want to design a cpu board with T1042 processor that use a 32 bits DDR3 SDRAM.  I do not know anything about its SDK.

because the T1040RDB use a 64bits DDR3 SDRAM and I use a 32 bits, I do not know what problems being in this way.

any body can describe these to problems to me.

thanks

ラベル(1)
0 件の賞賛
1 返信

372件の閲覧回数
ufedor
NXP Employee
NXP Employee

No additional precautions have to be done if SPD EEPROM (address 0x51 connected to the I2C1) with correct data is present.

Please refer to the following U-Boot source files:

/include/configs/T104xRDB.h

/drivers/ddr/fsl/ddr3_dimm_params.c

/drivers/ddr/fsl/main.c

0 件の賞賛