booting vxworks using uboot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

booting vxworks using uboot

5,053 Views
pritokhatri
Contributor I

Hi all,

i want to boot vxworks using uboot for t2080rdb board.

i download image over tftp at 0x1000000

gave bootvx 1000000

=> bootvx 1000000

## Ethernet MAC address not copied to NV RAM

## Using bootline (@ 0x4200): root=/dev/ram rw console=ttyS0,115200

## Starting vxWorks at 0x00100000 ...

but the log hangs after this.

am i doing anything wrong???

i also wanted to know whether the control has jump to vxworks or still its in uboot????

Labels (1)
0 Kudos
Reply
3 Replies

3,239 Views
elsasnow
Contributor II

On my issue, yes.

NXP changed SoDIMM vendors for rev C of the T2080RDB.

This requires some slight changes to the SPD parameters, which are hardcoded into the BSP.

The BSP works on some boards without changes, but requires the change on others, so the timing problem is right on the edge, I'm thinking.

I'm able to boot straight into VxWorks, bypassing U-boot entirely.

0 Kudos
Reply

3,239 Views
leotao
Contributor I

Have figured it out?

0 Kudos
Reply

3,239 Views
elsasnow
Contributor II

I'm having exactly the same problem on the T2080RDB.

Trying to get VxWorks 6.9.4 booted through U-Boot.

Same results as OP.


Can anyone help?

0 Kudos
Reply