like we want to use eth-3 or eth-4 ports in our application for transmit and receive data so how we can use that ports ?
is there any reference manual for that ?
and my second doubt is that how we can use DPAA for that ports ?
Hello jay loliyana,
What target board or processor are you using?
Did you developed Linux application or bareboard application? If so, your could refer to busy box ping application.
DPAA (Data Path Acceleration Architecture) hardware inspects ingress traffic and extracts user defined flows from the port traffic. It then steers specific flows (or related traffic) to a specific core or set of cores.
DPAA driver is enabled in Linux Kernel by default.
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
i m using bare-board application sir .
as you said that by busy box ping application what is that ?
how can i find that application n how we can use that ethernet port .