X T-2080 QDS Board vs. fsl_t2080_qds in vxWorks 6.9 BSP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

X T-2080 QDS Board vs. fsl_t2080_qds in vxWorks 6.9 BSP

2,177 Views
daeilkang
Contributor I

Dear All

I want to use fsl_t2080_qds BSP in the vxWorks 6.9 version with X T-2080 QDS board without any modification.

The board says the below information.

SCH-28012 REV A4

700-28012 REV A

X-T2080-QDS

The vxWorks 6.9 BSP says the below information.

SCH-28012 REV A3

700-28012 Rev X6

Freescale XT2080QDS

I programmed the default bootrom into X-T2080-QDS board.

But it doesn not work, I could see nothing on the serial terminal.

Can I use this vxWorks 6.9 BSP with this QDS board?

If no, please let me know which part is different between QDS board and this vxWorks BSP.

Thanks in advance

Kang

Labels (1)
Tags (2)
0 Kudos
Reply
2 Replies

1,229 Views
chilliar
Contributor I

Can anyone explain what the "700" means in the revisions?  I know the SCH means "Scheme", but there is nothing explaining what the "700" means in the revisions.

SCH-28012 REV A3 (scheme)

700-28012 Rev X6 (????)

0 Kudos
Reply

1,682 Views
Pavel
NXP Employee
NXP Employee

Difference between the T2080QDS Rev A3 and Rev A4 is the following:

The T2080 DUT all underneath decoupling capacitors are replaced for 2.2uF instead of 0.22uF.

See the Sheet 11 of the T2080QDS schematic.

It looks like that VxWorks should be used on the T2080QDS Rev A3 and Rev A4.

Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply