What is the purpose of PAMU if we use only single core in T2081

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What is the purpose of PAMU if we use only single core in T2081

2,547 次查看
manishraturi
Contributor I

Hi Team,

I am new to the community and new to T-series processors. I would like to know the purpose of PAMU.

Thanks & Regards

Manish Raturi

标签 (2)
0 项奖励
回复
2 回复数

2,282 次查看
bpe
NXP Employee
NXP Employee

PAMU is an analog of MMU, but for peripherals which can act as transaction initiators on the internal bus.

It isolates one bus master from another, restricting their memory access to areas defined by software.

PAMU is necessary for virtualization, if there is a requirement that virtual machines: (a) Utilise DMA-enabled

peripherals; (b) have to run in  isolated and controlled memory areas.

Even if you are going to use a single core, but wish to run several virtual machines, which can share

the core, but need to be isolated from one another in memory, PAMU may still be necessary.

If your application does not require virtualization, you can leave PAMU intact.

Refer to T2080RM, Chapter 11 for more information.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,282 次查看
scottwood
NXP Employee
NXP Employee

Without virtualization, the PAMU still plays a minor role, as it is required to enable DPAA stashing.

0 项奖励
回复