From the User Guide I see this -
Memory subsystem:
• SDRAM
• 3 DIMM slots, supports 2 GB per DIMM
• Supports DDR3 1866 UDIMM/RDIMM
But on my actual board that I bought it came to me pre-populated with 3 DIMMS and each of them was 8GBs each. And post bring up I see -
root@t4240rdb:~# free -h
total used free shared buff/cache available
Mem: 23G 66M 23G 844K 103M 23G
Swap: 0B 0B 0B
I want to know what is the maximum amount of RAM that I can populate, bring up and utilize on the T4240RDB.
Thanks,
Elliot
At a maximum it is possible to install 3x 64GB four-rank DIMMs.
Considering that the T4240RDB DIMM slots use only two chip-selects (ranks), available will be only half of each DIMM.