What is the config data required to enable the TMU in the T1022?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the config data required to enable the TMU in the T1022?

981 Views
Larry5335
Contributor IV

In the Reference Manual, it states that Freescale/NXP will provide the config data to use the TMU on the T1022, see below.

How can I get this?

33.2.14 TMU sensor configuration register (TMU_TSCFGR)

The TMU sensor configuration register, in conjunction with the temperature

configuration register, is used to initialize the internal sensor translation table used during

monitoring. Reading this register will return the data from the translation table as defined

by TTCFGR. Freescale provides the data required.

Labels (1)
Tags (1)
0 Kudos
2 Replies

727 Views
alexander_yakov
NXP Employee
NXP Employee

Please refer section 33.4 "Initialization Information" in the reference manual. It has all the required data.

Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

727 Views
Larry5335
Contributor IV

Yes, the revision 1 and newer Reference Manuals have section 33.4. Earlier revisions did not.

0 Kudos