Want to know the importance of these images to proceed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Want to know the importance of these images to proceed

692 Views
vinothkumars
Senior Contributor IV

Dear NXP,

I am working on T4160RDB-64B machine. I want to know some of the image specification. I don't the importance of these images.

https://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf

From this link (Table 110. NOR Flash Memory Map), 

0xEFE00000 0xEFE3FFFF CORTINA PHY code (current bank) 256KB

0xE8700000 0xE87FFFFF HV.uImage (current bank) 1MB

0xE8900000 0xE89FFFFF HV config device tree (current bank) 1MB

0xE8A00000 0xE8CFFFFF Guest image #1 (current bank) 3MB

0xE8D00000 0xE8FFFFFF Guest image #2 (current bank) 3MB

0xE9000000 0xE92FFFFF Guest image #3 (current bank) 3MB

Please provide the necessity of these images.

May I want to flash these all images or these are the options ?

Should I flash these images ?

Thanks & Regards,

VInothS

Regards,
Vinothkumar Sekar
Labels (1)
Tags (2)
0 Kudos
Reply
5 Replies

549 Views
bpe
NXP Employee
NXP Employee
CORTINA PHY codePHY firmware. Required if the board has this PHY,
unnecessary otherwise.
HV.uImage, HV config device tree

NXP Hypervisor images. Required if you are working
with NXP virtualization technologies, details can be found in
QorIQ SDK V2.0-1703 Documentation, Section 11.1. Not

required in the basic Linux boot scenario.

Guest image #1 - Guest image #3Hypervisor guest OS images. See above.


Have a great day,
Platon

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

549 Views
vinothkumars
Senior Contributor IV

Hi bpe,

I am using e6500 rev2 core support and this is the virtual core to T4160RDB processor.

So, I will flash the NXP Hypervisor images also.

Is it right ?

 

Thanks & Regards,

VinothS

Regards,
Vinothkumar Sekar
0 Kudos
Reply

549 Views
bpe
NXP Employee
NXP Employee

Yes, it is right


Have a great day,
Platon

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

549 Views
vinothkumars
Senior Contributor IV

Thank you bpe for the quick response,

Thanks & Regards,

VinothS 

Regards,
Vinothkumar Sekar
0 Kudos
Reply

549 Views
vinothkumars
Senior Contributor IV

Thank you Bpe,

I have e6500 rev2 core support also for this I want to flash HV.uImage, HV config device tree also.

Regards,

VinothS

Regards,
Vinothkumar Sekar
0 Kudos
Reply