UBOOT for T2080QDS Refrence board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UBOOT for T2080QDS Refrence board

1,441 Views
manishraturi
Contributor I

Hi Team,

We are trying to adopt the T2080QDS reference board u-boot code for our customized board. In reference board from freescale has the QIXIS FPGA MAPPED and its functionality is used in many places, is there a way where we can remove this functionality with removing some MACRO definition in U-BOOT. Because we will be using our FPGA and we will MAP our fpga address where currently QIXIS is mapped.

Thanks & Regards

Manish Raturi

Labels (1)
0 Kudos
Reply
1 Reply

1,107 Views
Pavel
NXP Employee
NXP Employee

Use the T2080RDB board as reference for your board. The T2080RDB does not have QIXIS.

If the T2080QDS board is used as reference for your board, change the code in the following folder:

/QorIQ-SDK-V1.9-20151210-yocto/build_t2080qds/tmp/work/t2080qds-fsl-linux/u-boot-qoriq/2015.01+fslgit-r0/git/board/freescale/t208xqds.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply