The T208x processors are or will be compatible with debian ppc64el?

cancel
Showing results for 
Search instead for 
Did you mean: 

The T208x processors are or will be compatible with debian ppc64el?

1,226 Views
robertoinnocent
Contributor III

We know that that e6500 core have Altivec running only in Big Endian mode, but debian ppc64el (little endian) its compiled with vmx extension that is the IBM altivec extension.

Debian 9 will be release for ppc64el and not for ppc64be or powperpc ( 32bit) so it means that it not run on e6500 core.

Future e6500 core or others Power Architecture NXP processor will have altivec an vmx compatibility even in Little Endian?

Labels (2)
3 Replies

593 Views
alexander_yakov
NXP Employee
NXP Employee

Sorry, for this particular moment we do not have any information about further e6500 core versions, or other Power Architecture further cores backward compatible with e6500.

Here is a direct link to product roadmap from recent FTF forum:

FTF-NET-N1863 What's Next for QorIQ - Portfolio and Roadmap.pdf 


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

593 Views
robertoinnocent
Contributor III

As all the GNU/Linux powerpc distro now run only with little endian and Altivec/VMX acceleration could you make an update of e6500 cores to support Altivec in Little endian? Do you need only to update the micro firmware of the e6500 core?

0 Kudos

593 Views
robertoinnocent
Contributor III

Any news about?

0 Kudos