According to the e5500 core reference manual, there is a TLB1 entry present after reset. It also states that the upper 6 bits of the Real Page Number (RPN) are applied to the core by SoC. However, I couldn't find specific details about these 6 bits in T1040 reference manual. Could you clarify what these 6-bit values are for T1040 SoC? This information might be helpful to add to T1040 SoC documentation if it is missing.
Thank you.
已解决! 转到解答。
@yipingwang thanks for the information, but could you please refer to where you found it in the reference manual? because I also knew it should be '00011" but it is not stated in the reference manual. please refer to the section in the reference manual.