TLB1 Entry 0 Values after Reset (e5500 core)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

TLB1 Entry 0 Values after Reset (e5500 core)

跳至解决方案
1,008 次查看
love_hate_and_repeat
Contributor III

According to the e5500 core reference manual, there is a TLB1 entry present after reset. It also states that the upper 6 bits of the Real Page Number (RPN) are applied to the core by SoC. However, I couldn't find specific details about these 6 bits in T1040 reference manual. Could you clarify what these 6-bit values are for T1040 SoC? This information might be helpful to add to T1040 SoC documentation if it is missing.

Thank you.

0 项奖励
回复
1 解答
913 次查看
yipingwang
NXP TechSupport
NXP TechSupport

I got this information from our internal data base provided by the AE team.

在原帖中查看解决方案

0 项奖励
回复
5 回复数
959 次查看
yipingwang
NXP TechSupport
NXP TechSupport

The default RPN[28-51] in TLB1 entry0 after reset is fffff. So RPN[28-33] is "000011".

0 项奖励
回复
949 次查看
love_hate_and_repeat
Contributor III

@yipingwang thanks for the information, but could you please refer to where you found it in the reference manual? because I also knew it should be '00011" but it is not stated in the reference manual. please refer to the section in the reference manual.

0 项奖励
回复
914 次查看
yipingwang
NXP TechSupport
NXP TechSupport

I got this information from our internal data base provided by the AE team.

0 项奖励
回复
886 次查看
love_hate_and_repeat
Contributor III
Why this information is not available in t1040 reference manual. This info can be added to the manual for its next revision.

Thanks.


0 项奖励
回复
851 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Thanks for your suggestion, we will do.

0 项奖励
回复