TLB1 Entry 0 Values after Reset (e5500 core)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TLB1 Entry 0 Values after Reset (e5500 core)

Jump to solution
1,232 Views
love_hate_and_repeat
Contributor III

According to the e5500 core reference manual, there is a TLB1 entry present after reset. It also states that the upper 6 bits of the Real Page Number (RPN) are applied to the core by SoC. However, I couldn't find specific details about these 6 bits in T1040 reference manual. Could you clarify what these 6-bit values are for T1040 SoC? This information might be helpful to add to T1040 SoC documentation if it is missing.

Thank you.

0 Kudos
Reply
1 Solution
1,137 Views
yipingwang
NXP TechSupport
NXP TechSupport

I got this information from our internal data base provided by the AE team.

View solution in original post

0 Kudos
Reply
5 Replies
1,183 Views
yipingwang
NXP TechSupport
NXP TechSupport

The default RPN[28-51] in TLB1 entry0 after reset is fffff. So RPN[28-33] is "000011".

0 Kudos
Reply
1,173 Views
love_hate_and_repeat
Contributor III

@yipingwang thanks for the information, but could you please refer to where you found it in the reference manual? because I also knew it should be '00011" but it is not stated in the reference manual. please refer to the section in the reference manual.

0 Kudos
Reply
1,138 Views
yipingwang
NXP TechSupport
NXP TechSupport

I got this information from our internal data base provided by the AE team.

0 Kudos
Reply
1,110 Views
love_hate_and_repeat
Contributor III
Why this information is not available in t1040 reference manual. This info can be added to the manual for its next revision.

Thanks.


0 Kudos
Reply
1,075 Views
yipingwang
NXP TechSupport
NXP TechSupport

Thanks for your suggestion, we will do.

0 Kudos
Reply