Hello,
We are using Nand flash with part no: MT29F128G08CBCEB.
IFC_CS1_B/GPIO2_10 of IFC INTERFACE is connected to CE0_0# and CE1_0# of nand flash.
IFC_CS2_B/GPIO2_11 of IFC INTERFACE is connected to CE0_1# and CE1_1# of nand flash.
Followed the instructions as per https://community.nxp.com/t5/Layerscape-Knowledge-Base/IFC-Controller-Configuration-on-QorIQ-Custom-... and configured the flash with the following parameters in u-boot.
updated the excel values as per the data sheet parameters
| SNo | Memory Model | tcls | tcs | twp | tdh | twh | trr | trp | trea | treh | twhr | twb | tadl | trc | twc | trhz | pagePerBlock | pageDataSize | pageSpareSize | MLCdevice | dataio | BlockCount | EDO | trhoh (toh) | trloh | trp(mod) | tww |
| 1 | MT29F128G08CBCEB | 50 | 70 | 50 | 5 | 11 | 20 | 50 | 40 | 30 | 120 | 200 | 150 | 100 | 100 | 200 | 512 | 16384 | 2208 | 1 | 8 | 8192 | 50 | 0 | 0 | 50 | 100 |
| S.No. | Register -> | FTIM0 | FTIM1 | FTIM2 | FTIM3 | Data Eye | FTIM0 | FTIM0 | FTIM1 | FTIM1 | FTIM2 | FTIM2 | CSPR0 | CS0R | NandMon | CSPR0 | CSOR | | |
| Memory Model | TCCST | TWP | TWCHT | TWH | TADLE | TWBE | TRR | TRP | TRAD | TREH | TWHRE | TWW | | NB0 | NB1 | NB2 | NB3 | [0:31] | NB0 | NB1 | NB2 | NB3 | [0:31] | [0:31] | [0:31] | [0:31] | [0:31] | [16:31] | RAL | PGS | SPRZ | PB | Trea | PS | THRZ | | |
| 1 | MT29F128G08CBCEB | 7 | 30 | 2 | 4 | 40 | 63 | 7 | 24 | 15 | 10 | 36 | | 2 | 0E | 1E | 02 | 04 | 0E1E0204 | 28 | 3F | 07 | 18 | 283F0718 | 01E | 050 | 24 | 01E05024 | 0083 | 01 | 11 | 111 | 100 | 14 | 01 | 011 | | |
#define CONFIG_SYS_NAND_BASE 0xff800000
#define CONFIG_SYS_NAND_BASE_PHYS (0xf00000000ull | CONFIG_SYS_NAND_BASE)
#define CONFIG_SYS_NAND_CS2_BASE 0xff810000
#define CONFIG_SYS_NAND_CS2_BASE_PHYS (0xf00000000ull | CONFIG_SYS_NAND_CS2_BASE)
#define CONFIG_SYS_NAND_CSPR_EXT (0x0)
#define CONFIG_SYS_NAND_CSPR (CSPR_PHYS_ADDR(CONFIG_SYS_NAND_BASE_PHYS) \
| CSPR_PORT_SIZE_8 /* Port Size = 8 bit */ \
| CSPR_MSEL_NAND /* MSEL = NAND */ \
| CSPR_V)
#define CONFIG_SYS_NAND_CS2_CSPR_EXT (0xf)
#define CONFIG_SYS_NAND_CS2_CSPR (CSPR_PHYS_ADDR(CONFIG_SYS_NAND_CS2_BASE_PHYS) \
| CSPR_PORT_SIZE_8 /* Port Size = 8 bit */ \
| CSPR_MSEL_NAND /* MSEL = NAND */ \
| CSPR_V)
#define CONFIG_SYS_NAND_AMASK IFC_AMASK(512*1024*16)
#define CONFIG_SYS_NAND_CSOR (CSOR_NAND_ECC_ENC_EN /* ECC on encode */ \
| CSOR_NAND_ECC_DEC_EN /* ECC on decode */ \
| CSOR_NAND_ECC_MODE_8 /* 8-bit ECC */ \
| CSOR_NAND_RAL_3 /* RAL = 3Bytes */ \
| CSOR_NAND_PGS_8K /* Page Size = 16K as per nand datasheet*/ \
| CSOR_NAND_SPRZ_CSOR_EXT /* Spare size */\
| CSOR_NAND_PB(512)) /*Page Per Block = 512*/
#define CONFIG_SYS_NAND_CSOR_EXT 0x000008A0
#define CONFIG_SYS_NAND_ONFI_DETECTION
/* ONFI NAND Flash mode0 Timing Params with reference to RDB*/
#define CONFIG_SYS_NAND_FTIM0 (FTIM0_NAND_TCCST(0x07) | \
FTIM0_NAND_TWP(0x1E) | \
FTIM0_NAND_TWCHT(0x02) | \
FTIM0_NAND_TWH(0x04))
#define CONFIG_SYS_NAND_FTIM1 (FTIM1_NAND_TADLE(0x28) | \
FTIM1_NAND_TWBE(0x3F) | \
FTIM1_NAND_TRR(0x07) | \
FTIM1_NAND_TRP(0x18))
#define CONFIG_SYS_NAND_FTIM2 (FTIM2_NAND_TRAD(0x0f) | \
FTIM2_NAND_TREH(0x0a) | \
FTIM2_NAND_TWHRE(0x24))
#define CONFIG_SYS_NAND_FTIM3 0x0
#define CONFIG_SYS_NAND_DDR_LAW 11
#define CONFIG_SYS_NAND_BASE_LIST {CONFIG_SYS_NAND_BASE,CONFIG_SYS_NAND_CS2_BASE}
#define CONFIG_SYS_MAX_NAND_DEVICE 2
#define CONFIG_CMD_NAND
#define CONFIG_SYS_NAND_BLOCK_SIZE (8192 * 1024)
Getting "Failed to detect ONFI extended param page" Error from U-Boot.
Here are prints from u-boot
U-Boot 2016.01-19722-ga9b437f-dirty (Jan 12 2022 - 15:47:53 +0530)
CPU0: T4241, Version: 2.0, (0x82400020)
Core: e6500, Version: 2.0, (0x80400120)
Clock Configuration:
CPU0:1800 MHz, CPU1:1800 MHz, CPU2:1800 MHz, CPU3:1800 MHz,
CPU4:1800 MHz, CPU5:1800 MHz, CPU6:1800 MHz, CPU7:1800 MHz,
CPU8:1800 MHz, CPU9:1800 MHz, CPU10:1800 MHz, CPU11:1800 MHz,
CCB:600 MHz,
DDR:800 MHz (1600 MT/s data rate) (Asynchronous), IFC:150 MHz
FMAN1: 700 MHz
FMAN2: 600 MHz
QMAN: 300 MHz
PME: 466.667 MHz
L1: D-cache 32 KiB enabled
I-cache 32 KiB enabled
Reset Configuration Word (RCW):
00000000: 0c080012 0e12120e 00000000 08000000
00000010: 04360848 30547a00 ec03f000 f9000000
00000020: 00080000 00000000 00000000 0003f000
00000030: 00000000 50000000 00000000 00000038
I2C: ready
Board: T4241, SERDES Reference Clocks:
SERDES1=125MHz SERDES2=125MHz
SERDES3=100MHz SERDES4=100MHz
SPI: ready
DRAM: Initializing DDR
10 GiB left unmapped
12 GiB (DDR3, 64-bit, CL=11, ECC on)
Value From Fuse Register = 10250
Corresponding value to be Written = 42
VID Write Successfull
Flash: 256 MiB
L2: 2 MiB enabled
enable l2 for cluster 1 fec60000
enable l2 for cluster 2 feca0000
Corenet Platform Cache: 1.5 MiB enabled
Using SERDES1 Protocol: 1 (0x1)
Using SERDES2 Protocol: 27 (0x1b)
Using SERDES3 Protocol: 1 (0x1)
Using SERDES4 Protocol: 9 (0x9)
fsl_ifc_cmdfunc: error, unsupported command 0x5.
fsl_ifc_read_buf beyond end of buffer (48 requested, 0 available)
fail in the CRC.
Failed to detect ONFI extended param page
No NAND device found
16384 MiB
MMC: FSL_SDHC: 0
PCIe1: Root Complex, x1 gen1, regs @ 0xfe240000
01:00.0 - 10ee:7011 - Multimedia device
PCIe1: Bus 00 - 01
PCIe3: Root Complex, no link, regs @ 0xfe260000
PCIe3: Bus 02 - 02
In: serial
Out: serial
Err: serial
Net: Fman1: Uploading microcode version 108.4.5
Could not get PHY for FM_TGEC_MDIO: addr 16
Failed to connect
Fman2: Uploading microcode version 108.4.5
FM1@TGEC1, FM2@DTSEC5 [PRIME], FM2@DTSEC6, FM2@DTSEC9, FM2@DTSEC10
POST Start:
POST Complete
U-boot Software Version : 1.0
tap env addr 0
Updating Boot Status Successful
Hit any key to stop autoboot: 0
T4241_uboot>
Thanks,
Balaji.G