Hello,
I have been experiencing some solder joint fractures on a board with T4241. I want to do an analysis to check if the thermal interface material we use exerts excessive mechanical pressure on the BGA when compressed.
What is the maximum initial (one-time) and sustained mechanical pressure that can be applied on the BGA? I found in the datasheet that the spring force (if using spring attached heatsink) should not exceed 270N, but is this the initial load value, or the sustained load?
Thanks,
Michal
Please refer to the following update from the AE team.
I checked with the packaging team and they informed me that the 270N is sustained load. We do not specify initial one-time load.