T4240: connect with BCM5396: The CPU side should be configured as serdes or sgmii?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T4240: connect with BCM5396: The CPU side should be configured as serdes or sgmii?

1,617 Views
carlpeng
Contributor II

Hello,

Could you please help to give some suggestions?

My question is as below:

In my designation, T4240's serdes interface is connected with a network switch BCM5396? then what attributes should the

serdes interface of T4240 side configure as, serdes or sgmii?

Thanks!

Labels (1)
0 Kudos
Reply
2 Replies

1,280 Views
carlpeng
Contributor II

Hello Lunmin,

Thanks a lot for your answer!

On BCM5396 side, the interface can be configured as serdes mode or sgmii mode, and on T4240 side, the serdes interface also

can be set as serdes mode and sgmii mode.

But as my understand, SGMII is a interface between MAC and phy, butthe connection between BCM5396 and T4240 is not the relationship of MAC and phy, but serdes and serdes, so I doubt if I set it as SGMII mode, it will not work.

Thank you!

0 Kudos
Reply

1,280 Views
lunminliang
NXP Employee
NXP Employee

Hello carl peng,

Serdes could be configured as several Networking protocols, such as XAUI, XFI SGMII, RGMII(LVCMOS pins) and so on, .  But what do you mean by "serdes or sgmii"?

I think you could check the interface type on BCM5396.

Regards

Lunmin

0 Kudos
Reply