T4240 10GB SFP+ Ethernet Performance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T4240 10GB SFP+ Ethernet Performance

392 Views
pedronavarro
Contributor I

We are using the driver provided by  vxWorks 6.9.4.7. 

We have a board that has the T4240 processor from NXP (formerly Freescale) 

This board has a 10GBp SFP+ ethernet interface. 

We are using IPerf software to evaluate performance. We have tested the performance without and with Jumbo Frames.in TCP. 

Without Jumbo Frames the performance is around 1.60GBbps. 

With Jumbo Frames the performance i around 5Gbps. 

Is it normal that performance?

Which are the recommendations to achieve better performance?

0 Kudos
1 Reply

264 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Pedro Navarro,

Please refer to the following 24C20G TCP Stream Jumbo Netperf performance on T4240RDB(Inbound ad Outbound).

FrameSize(Bytes)         Throughput(Mbps)

64                                  24287.7

1518                              29907.1

65536                            28208.1

Please refer to the following 24C20G TCP Stream Netperf performance on T4240RDB(Inbound ad Outbound)

FrameSize(Bytes)         Throughput(Mbps)

64                                  19720.5

1518                               22475.6

65536                             22577.1


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos