T4160RDB hang issue

cancel
Showing results for 
Search instead for 
Did you mean: 

T4160RDB hang issue

Jump to solution
531 Views
vinothkumars
Senior Contributor III

Hi All,

   We have a custom board built with T4160RDB processor. I am facing the issue where uboot hangs. u-boot hang when reboot command issued from Linux console. But, it will work when normal power on and off sequence mean boots normally,  What could be the issue?

Regards, VinothS

Regards,
Vinothkumar Sekar
0 Kudos
1 Solution
273 Views
ufedor
NXP TechSupport
NXP TechSupport

You wrote:

> We have a custom board built with T4160RDB processor.

T4160?

Or T4240RDB board?

The Linux reboot is implemented using the RSTCR register - refer to the /arch/powerpc/sysdev/fsl_soc.c

Please check how RESET_REQ_B assertion is handled in your hardware.

View solution in original post

0 Kudos
4 Replies
274 Views
ufedor
NXP TechSupport
NXP TechSupport

You wrote:

> We have a custom board built with T4160RDB processor.

T4160?

Or T4240RDB board?

The Linux reboot is implemented using the RSTCR register - refer to the /arch/powerpc/sysdev/fsl_soc.c

Please check how RESET_REQ_B assertion is handled in your hardware.

View solution in original post

0 Kudos
273 Views
vinothkumars
Senior Contributor III

Hi Ufedor,

Thank you for the reply. This the problem with hardware. Reboot works after implementing the RESET_REQ_B in Hardware side.

Thanks,

VinothS.

Regards,
Vinothkumar Sekar
0 Kudos
273 Views
vinothkumars
Senior Contributor III

Ufedor,

Thank you for your reply.

I am using T4160RDB-64B machine only.

So, for reboot from Linux console want to do the RSTCR register configuration in Linux side.

 

Regards, Vinoth

Regards,
Vinothkumar Sekar
0 Kudos
273 Views
vinothkumars
Senior Contributor III

Currently close this thread. This is the problem with loading FMAN binary code.

Regards,

VinothS

Regards,
Vinothkumar Sekar
0 Kudos