T208x SRDS_PRTCL_S1 how to set?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T208x SRDS_PRTCL_S1 how to set?

898件の閲覧回数
gyosunshim
Contributor III

Hi All,

Use the T2080RDB evm board has designed the T2081 board.

SRDS_PRTCL_S1 value of T2080RDB is called to change this value to 0x66 0x6C.

How do I change the value?

Note also the boot to SD.

Thank you.

Best regards,

gyosun

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

697件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Hello gyosun shim,

Seems the question is not very clear.

The SRDS_PRTCL_S1is RCW field for setting Serdes protocol, please refer to Table 19-1 for SerDes Lanes Assignments.

You mentioned 0x66 0x6C, do you want to set one of this value?

You could use the QCVS tool to change this part in RCW and generate image.

Please correct me if this is not what you're asking about.


Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

697件の閲覧回数
gyosunshim
Contributor III

Hello lunminliang,

Please note that this question did not smooth.

I want to set the value to SRDS_PRTCL_S1 0x6c.

If QCVS tools have made the bin file, how do I download on u-boot?

I am using an SD card to boot.

Thank you,

Best regards,

gyosun

0 件の賞賛
返信