T2081: U-boot not responding after entering key to stop the autoboot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T2081: U-boot not responding after entering key to stop the autoboot

ソリューションへジャンプ
4,223件の閲覧回数
noufalp90
Contributor III

Hi Team,

 

One of our custom board uses T2081QDS SOC with 4GB of DDR. Currently we are able to port u-boot on the custom board and stop the autoboot at u-boot by pressing any key. But we are not able to execute any commands on the u-boot console. We can say it is receiving only the key to stop the autoboot but no other commands from the user. Can you please guide me with the solution or areas to check to resolve this issue?

 

Thanks,

Noufal

 

T2080 Screenshot (66).png#t2081QD

ラベル(1)
0 件の賞賛
返信
1 解決策
3,986件の閲覧回数
noufalp90
Contributor III

Hi @LFGP 

There is no issue with the RAM as seen in the boot log. PFA complete boot log. image (2).png

 

We are also suspecting Processor UART-RX line. Debug is going on.

Thanks, 

Noufal

元の投稿で解決策を見る

0 件の賞賛
返信
7 返答(返信)
4,087件の閲覧回数
LFGP
NXP TechSupport
NXP TechSupport

dear @noufalp90 ,

let it continue with the boot process, don't hit any key, and share, on this way,  a complete log file.

I want to check if there some message about RAM or DTS.

0 件の賞賛
返信
3,987件の閲覧回数
noufalp90
Contributor III

Hi @LFGP 

There is no issue with the RAM as seen in the boot log. PFA complete boot log. image (2).png

 

We are also suspecting Processor UART-RX line. Debug is going on.

Thanks, 

Noufal

0 件の賞賛
返信
4,142件の閲覧回数
LFGP
NXP TechSupport
NXP TechSupport

I see you are booting from NOR, right? , so, as a test please remove the SD card (if you have one) and any peripherical device. 

0 件の賞賛
返信
4,131件の閲覧回数
noufalp90
Contributor III
Yes, We are booting from NOR. We dont have any SD card. You meant to say removing peripheral from the u-boot config and try ?

Thanks
Noufal
0 件の賞賛
返信
4,192件の閲覧回数
LFGP
NXP TechSupport
NXP TechSupport

dear @noufalp90 ,

it is necessary to re-build the image, be sure you are using the Uboot adequate version regarding the SDK.

  

0 件の賞賛
返信
4,152件の閲覧回数
noufalp90
Contributor III
Hi,

Thank you for your suggestion. I have downloaded u-boot from https://github.com/nxp-qoriq/u-boot/tree/git.denx.de/u-boot-2016.09.y/ since the SDK document mentioned that updated version of the u-boot is 2016.09. Still we are stuck in the console.

Thank you.
Noufal
0 件の賞賛
返信
4,106件の閲覧回数
noufalp90
Contributor III

Hi @LFGP ,

 

I have disabled almost all other peripherals. But still not working. U-boot stuck after entering key to stop autoboot. 

PFA new boot log.

 

Thanks,

Noufal

 

0 件の賞賛
返信