Hi, Dear:
I'm developing T2080RDB-PC boards, and I have a bit of a problem when replacing the DDR3 memory card. The original DDR3L(D3XP56082XL10AA) can correctly identify memory under 1066Mhz/1600Mhz/1866Mhz, and the logs as follows:
“
U-Boot 2016.012.0+ga9b437f (Oct 26 2017 - 10:47:17 +0800)
initcall: eff4eee4
U-Boot code: EFF40000 -> F0000000 BSS: -> F004D4A0
initcall: eff4809c
CPU0: T2080E, Version: 1.1, (0x85380011)
Core: e6500, Version: 2.0, (0x80400120)
Clock Configuration:
CPU0:1799.820 MHz, CPU1:1799.820 MHz, CPU2:1799.820 MHz, CPU3:1799.820 MHz,
CCB:599.940 MHz,
DDR:799.980 MHz (1599.960 MT/s data rate) (Asynchronous), IFC:149.985 MHz
FMAN1: 699.930 MHz
QMAN: 299.970 MHz
PME: 599.940 MHz
L1: D-cache 32 KiB enabled
I-cache 32 KiB enabled
Reset Configuration Word (RCW):
00000000: 1206001b 15000000 00000000 00000000
00000010: 66150002 00000000 ec027000 c1000000
00000020: 00800000 00000000 00000000 000307fc
00000030: 00000000 00000000 00000000 00000004
initcall: eff4ebe0
initcall: eff4f088
I2C: Requested speed:100000, i2c_clk:299970000
FDR:0x34, div:5120, ga:0x4, gb:0x5, a:10, b:512, speed:58587
Tr <= 1566 ns
FDR:0x31, div:3072, ga:0x5, gb:0x4, a:12, b:256, speed:97646
Tr <= 713 ns
divider:2999, est_div:3072, DFSR:14
FDR:0x31, speed:97646
ready
initcall: eff4f904
Board: T2080RDB, Board rev: 0x01 CPLD ver: 0x03, boot from NOR vBank4
SERDES Reference Clocks:
SD1_CLK1=156.25MHZ, SD1_CLK2=100.00MHZ
SD2_CLK1=100.00MHZ, SD2_CLK2=100.00MHZ
initcall: eff4f048
SPI: ready
initcall: eff4f014
DRAM: initcall: eff4efb8
Initializing....using SPD
starting at step 1 (STEP_GET_SPD)
Requested speed:100000, i2c_clk:299970000
FDR:0x34, div:5120, ga:0x4, gb:0x5, a:10, b:512, speed:58587
Tr <= 1566 ns
FDR:0x31, div:3072, ga:0x5, gb:0x4, a:12, b:256, speed:97646
Tr <= 713 ns
divider:2999, est_div:3072, DFSR:14
FDR:0x31, speed:97646
DDR: DDR III rank density = 0x 80000000
Computing lowest common DIMM parameters for memctl=0
Detected UDIMM D3XP56082XL10AA
lowest_common_spd_caslat is 0xb
all DIMMs ECC capable
tCKmin_ps = 1071
trcd_ps = 13125
trp_ps = 13125
tras_ps = 34000
twtr_ps = 7500
trfc_ps = 160000
trrd_ps = 5000
twr_ps = 15000
trc_ps = 47125
Reloading memory controller configuration options for memctl=0
mclk_ps = 1250 ps
Found timing match: n_ranks 2, data rate 1600, rank_gb 2
clk_adjust 5, wrlvl_start 8, wrlvl_ctrl_2 0x808070b, wrlvl_ctrl_3 0xc0d0e0a
0 of 1 controllers are interleaving.
Checking interleaving options completed
dbw_cap_adj[0]=0
ctrl 0 dimm 0 base 0x0
ctrl 0 total 0x100000000
Total mem by __step_assign_addresses is 0x100000000
Total mem 4294967296 assigned
FSL Memory ctrl register computation
FSLDDR: cs[0]_bnds = 0x000000ff
FSLDDR: cs[0]_config = 0x80044302
FSLDDR: cs[0]_config_2 = 0x00000000
FSLDDR: cs[1]_bnds = 0x000000ff
FSLDDR: cs[1]_config = 0x80004302
FSLDDR: cs[1]_config_2 = 0x00000000
FSLDDR: cs[2]_bnds = 0x00000000
FSLDDR: cs[2]_config = 0x00000000
FSLDDR: cs[2]_config_2 = 0x00000000
FSLDDR: cs[3]_bnds = 0x00000000
FSLDDR: cs[3]_config = 0x00000000
FSLDDR: cs[3]_config_2 = 0x00000000
FSLDDR: timing_cfg_0 = 0x5011010c
FSLDDR: timing_cfg_3 = 0x01071000
FSLDDR: timing_cfg_1 = 0xbcb48c46
FSLDDR: timing_cfg_2 = 0x0040c156
FSLDDR: ddr_cdr1 = 0x80040000
FSLDDR: ddr_cdr2 = 0x00000001
FSLDDR: ddr_sdram_cfg = 0xc7054000
FSLDDR: ddr_sdram_cfg_2 = 0x24401100
FSLDDR: ddr_sdram_mode = 0x00441c70
FSLDDR: ddr_sdram_mode_3 = 0x00001c70
FSLDDR: ddr_sdram_mode_5 = 0x00001c70
FSLDDR: ddr_sdram_mode_5 = 0x00001c70
FSLDDR: ddr_sdram_mode_2 = 0x00980000
FSLDDR: ddr_sdram_mode_4 = 0x00980000
FSLDDR: ddr_sdram_mode_6 = 0x00980000
FSLDDR: ddr_sdram_mode_8 = 0x00980000
FSLDDR: ddr_sdram_interval = 0x0c30030c
FSLDDR: clk_cntl = 0x03000000
FSLDDR: timing_cfg_4 = 0x00000001
FSLDDR: timing_cfg_5 = 0x04401400
FSLDDR: zq_cntl = 0x89080600
FSLDDR: wrlvl_cntl = 0x8675f608
FSLDDR: wrlvl_cntl_2 = 0x0808070b
FSLDDR: wrlvl_cntl_3 = 0x0c0d0e0a
Programming controller 0
total 4 GB
Need to wait up to 66 * 10ms
setup ddr law base = 0x0, size 0x100000000, TRGT_ID 0x10
total_memory by __fsl_ddr_sdram = 4294967296
total_memory by __fsl_ddr_sdram = 4294967296
2 GiB left unmapped
initcall: eff4f2fc
Monitor len: 0010D4A0
Ram size: 00000000
Ram top: 80000000
Reserving MP boot page to 7ffff000
initcall: eff4ec2c
initcall: eff4ec40
initcall: eff4ee68
Reserving 1077k for U-Boot at: 7fef0000
initcall: eff4ee08
have goto reserve_malloc steps before!
Reserving 4104k for malloc() at: 7faee000
have goto reserve_malloc steps after!
initcall: eff4ef24
have goto reserve_board steps before!
sizeof(bd_t) = 72 Bytes, gd->start_addr_sp = 7faedfb8!
Reserving 72 Bytes for Board Info at: 7faedfb8
have goto reserve_board steps after!
initcall: eff4edd4
have goto setup_machine steps!
initcall: eff4ed70
have goto reserve_global_data steps before!
Reserving 192 Bytes for Global Data at: 7faedef8
have goto reserve_global_data steps after!
initcall: eff4ece8
initcall: eff4eca0
initcall: eff4f3cc
initcall: eff4f2bc
initcall: eff4f26c
4 GiB (DDR3, 64-bit, CL=11, ECC off)
DDR Chip-Select Interleaving Mode: CS0+CS1
”
But when I change the memory card to DDR3(RMT3150ED58E8W1600), the u-boot stopped and hanged. The log as follows:
“
U-Boot 2016.012.0+ga9b437f (Oct 26 2017 - 10:47:17 +0800)
initcall: eff4eee4
U-Boot code: EFF40000 -> F0000000 BSS: -> F004D4A0
initcall: eff4809c
CPU0: T2080E, Version: 1.1, (0x85380011)
Core: e6500, Version: 2.0, (0x80400120)
Clock Configuration:
CPU0:1799.820 MHz, CPU1:1799.820 MHz, CPU2:1799.820 MHz, CPU3:1799.820 MHz,
CCB:599.940 MHz,
DDR:799.980 MHz (1599.960 MT/s data rate) (Asynchronous), IFC:149.985 MHz
FMAN1: 699.930 MHz
QMAN: 299.970 MHz
PME: 599.940 MHz
L1: D-cache 32 KiB enabled
I-cache 32 KiB enabled
Reset Configuration Word (RCW):
00000000: 1206001b 15000000 00000000 00000000
00000010: 66150002 00000000 ec027000 c1000000
00000020: 00800000 00000000 00000000 000307fc
00000030: 00000000 00000000 00000000 00000004
initcall: eff4ebe0
initcall: eff4f088
I2C: Requested speed:100000, i2c_clk:299970000
FDR:0x34, div:5120, ga:0x4, gb:0x5, a:10, b:512, speed:58587
Tr <= 1566 ns
FDR:0x31, div:3072, ga:0x5, gb:0x4, a:12, b:256, speed:97646
Tr <= 713 ns
divider:2999, est_div:3072, DFSR:14
FDR:0x31, speed:97646
ready
initcall: eff4f904
Board: T2080RDB, Board rev: 0x01 CPLD ver: 0x03, boot from NOR vBank4
SERDES Reference Clocks:
SD1_CLK1=156.25MHZ, SD1_CLK2=100.00MHZ
SD2_CLK1=100.00MHZ, SD2_CLK2=100.00MHZ
initcall: eff4f048
SPI: ready
initcall: eff4f014
DRAM: initcall: eff4efb8
Initializing....using SPD
starting at step 1 (STEP_GET_SPD)
Requested speed:100000, i2c_clk:299970000
FDR:0x34, div:5120, ga:0x4, gb:0x5, a:10, b:512, speed:58587
Tr <= 1566 ns
FDR:0x31, div:3072, ga:0x5, gb:0x4, a:12, b:256, speed:97646
Tr <= 713 ns
divider:2999, est_div:3072, DFSR:14
FDR:0x31, speed:97646
DDR: DDR III rank density = 0x 80000000
Computing lowest common DIMM parameters for memctl=0
Detected UDIMM RMT3150ED58E8W1600
lowest_common_spd_caslat is 0xb
Warning: not all DIMMs ECC capable, cant enable ECC
tCKmin_ps = 1250
trcd_ps = 13125
trp_ps = 13125
tras_ps = 35000
twtr_ps = 7500
trfc_ps = 160000
trrd_ps = 6000
twr_ps = 15000
trc_ps = 48125
Reloading memory controller configuration options for memctl=0
mclk_ps = 1250 ps
Found timing match: n_ranks 1, data rate 1600, rank_gb 2
clk_adjust 5, wrlvl_start 8, wrlvl_ctrl_2 0x808070b, wrlvl_ctrl_3 0xc0d0e0a
0 of 1 controllers are interleaving.
Checking interleaving options completed
dbw_cap_adj[0]=0
ctrl 0 dimm 0 base 0x0
ctrl 0 total 0x80000000
Total mem by __step_assign_addresses is 0x80000000
Total mem 2147483648 assigned
FSL Memory ctrl register computation
FSLDDR: cs[0]_bnds = 0x0000007f
FSLDDR: cs[0]_config = 0x80044302
FSLDDR: cs[0]_config_2 = 0x00000000
FSLDDR: cs[1]_bnds = 0x00000000
FSLDDR: cs[1]_config = 0x00000000
FSLDDR: cs[1]_config_2 = 0x00000000
FSLDDR: cs[2]_bnds = 0x00000000
FSLDDR: cs[2]_config = 0x00000000
FSLDDR: cs[2]_config_2 = 0x00000000
FSLDDR: cs[3]_bnds = 0x00000000
FSLDDR: cs[3]_config = 0x00000000
FSLDDR: cs[3]_config_2 = 0x00000000
FSLDDR: timing_cfg_0 = 0x5011010c
FSLDDR: timing_cfg_3 = 0x01071000
FSLDDR: timing_cfg_1 = 0xbcb48c56
FSLDDR: timing_cfg_2 = 0x0040c158
FSLDDR: ddr_cdr1 = 0x80040000
FSLDDR: ddr_cdr2 = 0x00000001
FSLDDR: ddr_sdram_cfg = 0xc7050000
FSLDDR: ddr_sdram_cfg_2 = 0x24401100
FSLDDR: ddr_sdram_mode = 0x00441c70
FSLDDR: ddr_sdram_mode_3 = 0x00001c70
FSLDDR: ddr_sdram_mode_5 = 0x00001c70
FSLDDR: ddr_sdram_mode_5 = 0x00001c70
FSLDDR: ddr_sdram_mode_2 = 0x00980000
FSLDDR: ddr_sdram_mode_4 = 0x00980000
FSLDDR: ddr_sdram_mode_6 = 0x00980000
FSLDDR: ddr_sdram_mode_8 = 0x00980000
FSLDDR: ddr_sdram_interval = 0x0c30030c
FSLDDR: clk_cntl = 0x03000000
FSLDDR: timing_cfg_4 = 0x00000001
FSLDDR: timing_cfg_5 = 0x04401400
FSLDDR: zq_cntl = 0x89080600
FSLDDR: wrlvl_cntl = 0x8675f608
FSLDDR: wrlvl_cntl_2 = 0x0808070b
FSLDDR: wrlvl_cntl_3 = 0x0c0d0e0a
Programming controller 0
total 2 GB
Need to wait up to 32 * 10ms
setup ddr law base = 0x0, size 0x80000000, TRGT_ID 0x10
total_memory by __fsl_ddr_sdram = 2147483648
total_memory by __fsl_ddr_sdram = 2147483648
initcall: eff4f2fc
Monitor len: 0010D4A0
Ram size: 80000000
Ram top: 80000000
Reserving MP boot page to 7ffff000
initcall: eff4ec2c
initcall: eff4ec40
initcall: eff4ee68
Reserving 1077k for U-Boot at: 7fef0000
initcall: eff4ee08
have goto reserve_malloc steps before!
Reserving 4104k for malloc() at: 7faee000
have goto reserve_malloc steps after!
initcall: eff4ef24
have goto reserve_board steps before!
sizeof(bd_t) = 72 Bytes, gd->start_addr_sp = 7faedfb8!
”
I tried 1066Mhz and 1600Mhz, changed the SWITCH SETTING SW2[7] to 0(ON), and connect the Jumper J27(1.5V). And I tried all the DDR_DDR_SDRAM_CLK_CNTL phases. The phenomenon is the same.
And I tried to set DDR_TIMING_CFG_2[WR_DATA_DELAY] to 1/2 clock delay, it would not work too.
The Differences between these memory card is as followed:
And I think the T2080 ddr registers are setup automatically by reading eeprom in memory card.
It's been two weeks since I got stuck in this problem, and the memory card is fine. What is the problem?The Complete logs see attachments.
Looking forward to your reply.
Yours Yang
Solved! Go to Solution.
Hi:
I just only exchanged the T2080RDB-PC's memory card! Then, It can not work any more, What can I do now?
Hi:
I just only exchanged the T2080RDB-PC's memory card! Then, It can not work any more, What can I do now?
Your dump shows problem about ECC using for new DIMM. Test your board if ECC is enabled in the u-boot. Comment CONFIG_DDR_ECC variable in the /include/configs/T208xRDB.h file.
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Pavel:
Thanks for your reply. My new memory card(RMT3150ED58E8W1600) doesn't support the ECC. So I disabled the CONFIG_DDR_ECC variable. I have tried a lot of register combinations, however it does't work yet!
Have a good day! Yours Yang
Hi
The project is very urgent. Can someone provide help as soon as possible?
yours Yang