I run fra because I need test srio doorbell fuction,and I need modify some code of fra,but when I build fra by the command:"bitbake -c compile -f usdpaa-apps or bitbake usdpaa-apps",I can't get the modified fra excutalbe file,it just the one unmodified .The problem is also happened when I modifed SRA and usdpaa code.
so ,Is the build command not right ? or does the usdpaa and usdpaa-apps deny any modifies ?
Please refer to the following procedure.
$ bitbake usdpaa-apps -c cleansstate
$ bitbake usdpaa-apps -c patch
Go to folder build_t2080rdb/tmp/work/t2080rdb-fsl-linux/usdpaa-apps/git-r0/git/src/ to modify usdpaa-apps source code.
Then rebuild usdpaa-apps
$ bitbake usdpaa-apps
You will get the binaries in build_t2080rdb/tmp/work/t2080rdb-fsl-linux/usdpaa-apps/git-r0/image/