T2080 port trouble

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T2080 port trouble

973 Views
matiaslirman
Contributor II

Hello,

I have been working on the routing capabilities of the T2080 and have run into some issues regarding one of the 10G Ethernet ports on the board.

I cant seem to get any sort of connection from the port ETH0. Upon initialization, I try to configure the port to simply ping the computer that is connected to the port through a 10Gb Ethernet cable but I continually get the response: 

From 192.168.1.100 icmp_seq=1 Destination Host Unreachable

This port is the only one that has given me any issues. If I run the following commands after initialization for ETH1 (fm1-mac10) I get an appropriate response from the ping request:

ifconfig fm1-mac10 192.1681.100/24

ip link set fm1-mac10 up

ping 192.168.1.70 (the IP address to the connected computer)

I then restart the board and run the same commads for the ETH0 (fm1-mac9) port but get a different response from the ping request (shown above):

ifconfig fm1-mac9 192.1681.100/24

ip link set fm1-mac9 up

ping 192.168.1.70 (the IP address to the connected computer)

The TX and RX lights both turn on when the ethernet cable is inserted into the ETH0 port just like it does when inputted into the ETH1 port so it seems that a connection is read. Is there any reason why this should not be working; I am running the same commands but get different responses? I have tried the same thing with multiple cables and computers and keep getting the same issue. Is this a hardware issue? Any help would be greatly appreciated as I am completely stumped.

THANKS IN ADVANCE!

Best,

Matias Lirman 

Labels (1)
0 Kudos
Reply
1 Reply

758 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Matias Lirman,

Please enter u-boot prompt, and configure the parameters as the following, please check whether this 10G Ethernet port can work under u-boot.

=> setenv ethact FM1@TGEC1
=> setenv ipaddr 192.168.1.100
=> ping 192.168.1.70

In addition, would you please send the whole u-boot and Linux Kernel booting up log to me? I will do more investigation for you.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply