T2080 VCORE controller alternative?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

T2080 VCORE controller alternative?

2,067 次查看
davef
Contributor I

The 2-phase buck controller (IR36021) recommended for the T2080 core voltage supply (and implemented in the RDB) is obsolete.

Does NXP have a recommendation for a replacement controller that supports a manual VID programming facility (I2C or PMBUS)?

标签 (2)
0 项奖励
回复
3 回复数

1,917 次查看
abhijit_pethkar
Contributor II

Use LTM4676A from Linear Technology. We have used it in our design with T2081 Processor.

0 项奖励
回复

1,917 次查看
aneeshk
Contributor I

Hi,

Is there any suggestion for TI power controller module with external switch?

0 项奖励
回复

1,917 次查看
Pavel
NXP Employee
NXP Employee

There are no recommendations for replacing IR36021.

Use as Layerscape communications processor board schematic.

For example see the LS1088ARDB schematic:

https://www.nxp.com/downloads/en/printed-circuit-boards/LS1088ARDB-PB-DF.zip

 

This board uses the LTC3882 as buck converter.

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复