T2080 USB control signals

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T2080 USB control signals

799件の閲覧回数
paulagarcía-mor
Contributor I

If I don't use the USB power fault and usb power enable signals, would I have any problem with this interface?

I don't want to use them since I am using the same 5V regulator to supply USB and other devices, so I don't want USB controller to controls also those other devices.

Should I use a specific 5V source to USB so I can control it with the above mentioned signals or it is not necessary?

Thanks in advance.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

725件の閲覧回数
ufedor
NXP Employee
NXP Employee

It is possible to not use the signals in question, but the board designer still has to take precautions to eliminate possible hardware damage in case of USB device power failure.

0 件の賞賛
返信