There is a note at the beginning of the table.
"When selecting protocols from the table below, there is a restriction to choose
the supported protocol combinations by line (SerDes 1 and
SerDes 2 together), for example SRDS_PRCTL_S1= A2 can
ONLY be combined with SRDS_PRTCL_S2= 16."
So I choose SRDS_PRCTL_S1 = 0x6D and SRDS_PRTCL_S2 = 0x2D.
But in QCVS,there is only SRDS_PRCTL_S1 = 0x6C option.
I can only choose SRDS_PRCTL_S1 = 0x6C and SRDS_PRTCL_S2 = 0x2D.
Is it correct?
In addition,there is a warning reffer to A-007186 on SRDS_PRCTL_S1 in QCVS.
I have checked that A-007186 is reffer to SRIO 2.5 Gbaud or 5 Gbaud.
What does it mean?