T2080 Secure vs. Trusted

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

T2080 Secure vs. Trusted

跳至解决方案
2,577 次查看
dmitri_lechtchinski
Contributor III

The documentation describes two following security states: Trusted and Secure.

What is the functional difference between the two in this specific SoC, in terms of available mechanisms, violations behavior, available keys, etc.?

Is Secure considered to be "more secure", and if yes then in what way?

Are there any functionalities that are available in only one of the states?

Thanks,
Dmitri

标签 (1)
0 项奖励
回复
1 解答
2,573 次查看
ufedor
NXP Employee
NXP Employee

The modes are described in the QorIQ Trust Architecture 2.0 User Guide, 7.2.6.1.2 State definitions.

在原帖中查看解决方案

4 回复数
2,574 次查看
ufedor
NXP Employee
NXP Employee

The modes are described in the QorIQ Trust Architecture 2.0 User Guide, 7.2.6.1.2 State definitions.

2,564 次查看
dmitri_lechtchinski
Contributor III
This chapter doesn't really answer these questions.. I see no major difference between the two states, can you elaborate please? Additionaly, this document states in the mentioned chapter: "In the device, there is limited difference between Trusted and Secure State. This distinction is more relevant in other NXP devices that also use the security monitor." Does this mean that specifically in T2080 there is no functional difference between the two?
0 项奖励
回复
2,559 次查看
ufedor
NXP Employee
NXP Employee

Your understanding is correct.

2,554 次查看
dmitri_lechtchinski
Contributor III
Thanks!
0 项奖励
回复