T2080 Secure vs. Trusted

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T2080 Secure vs. Trusted

Jump to solution
2,599 Views
dmitri_lechtchinski
Contributor III

The documentation describes two following security states: Trusted and Secure.

What is the functional difference between the two in this specific SoC, in terms of available mechanisms, violations behavior, available keys, etc.?

Is Secure considered to be "more secure", and if yes then in what way?

Are there any functionalities that are available in only one of the states?

Thanks,
Dmitri

Labels (1)
0 Kudos
Reply
1 Solution
2,595 Views
ufedor
NXP Employee
NXP Employee

The modes are described in the QorIQ Trust Architecture 2.0 User Guide, 7.2.6.1.2 State definitions.

View solution in original post

4 Replies
2,596 Views
ufedor
NXP Employee
NXP Employee

The modes are described in the QorIQ Trust Architecture 2.0 User Guide, 7.2.6.1.2 State definitions.

2,586 Views
dmitri_lechtchinski
Contributor III
This chapter doesn't really answer these questions.. I see no major difference between the two states, can you elaborate please? Additionaly, this document states in the mentioned chapter: "In the device, there is limited difference between Trusted and Secure State. This distinction is more relevant in other NXP devices that also use the security monitor." Does this mean that specifically in T2080 there is no functional difference between the two?
0 Kudos
Reply
2,581 Views
ufedor
NXP Employee
NXP Employee

Your understanding is correct.

2,576 Views
dmitri_lechtchinski
Contributor III
Thanks!
0 Kudos
Reply