T2080 PCIe polarity reversal

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T2080 PCIe polarity reversal

Jump to solution
1,108 Views
tomsaluzzo
Contributor III

Please confirm T2080 supports PCIe polarity reversal on the RX port as per the PCIe spec. I couldn't find it documented in the T2080 documentation.

Labels (1)
0 Kudos
Reply
1 Solution
957 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
Reply
2 Replies
958 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
Reply
959 Views
Bulat
NXP Employee
NXP Employee

The T2080 PCI Express interface is compatible with the PCI Express Base Specification, Revision 3.0, this assumes that it supports all features from the specifications.

0 Kudos
Reply