Hello,
I have been implementing a time triggered routine on the T2080RDB PCA platform. I use the global timer A group, more precisely the timer 0.
I set the GTVPRA0 accordingly, the destination register to multicast on all cores. The CTPR is also correctly set for all cores (masks interrupts 0 to 14, my GTVPRA0 is set to have a priority of 15).
However, the interrupt is only triggered on the CPU 0 (I don't use SMT so only one thread is enabled).
I can't find where my mistake is. I am pretty sure I forgot to set a register somewhere, but the fact that the CPU 0 receives the interrupts bugs me. Also, this implementation was first done on the P2020 target (that uses a PIC, not an MPIC) and it worked like a charm.
I was wondering if anyone had an idea about what to check to fix this issue.
Best regards,
Alexy