T2080 MPIC_EISR values

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T2080 MPIC_EISR values

502 Views
dmitri_lechtchinski
Contributor III

Hello,

For MPIC_EISR register, is it possible for multiple bits to be set in the same received interrupt?

Or will each source be received as a separate interrupt with only one bit set, even if multiple sources are active at the same time?

Thank you,

Dmitri

 

Labels (1)
0 Kudos
1 Reply

488 Views
r8070z
NXP Employee
NXP Employee

Yes, it is possible for multiple bits of MPIC_EISR to be set in the same received interrupt (internal interrupt 0).

0 Kudos