T2080-Ethernet self IP-pinging with -I option is not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T2080-Ethernet self IP-pinging with -I option is not working

1,278 Views
soumyasephalika
Contributor I

Hi,

In T2080 processor, pinging by Ethernet port by -I option is working for other IP addresses connected to the network.

ping -I <Device name> <IP address>

While, Ethernet self IP-pinging with -I option is not working.

ping -I <Device name> <Self IP address>

But when we are self pinging without -I option by ping <Self IP address> command the Ethernet is pinging.

Kindly suggest the probable root cause for the above problem.

Regards

Soumya S

Hardware design Engineer

Labels (1)
0 Kudos
Reply
0 Replies