T2080 ATMU setup for PCIe1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T2080 ATMU setup for PCIe1

1,757 Views
scottgerhold
Contributor IV

I have 2 T2080s attached to each other on PCIe. I have 1 setup as the RC and the other setup as the EP. I am only testing traffic (reads/writes) to the EP from the RC. When I run the test for connections between PCIe2 or PCIe4 the test functions correctly and data written to the EP is echoed back correctly on reads from the EP. The test is simply mapping to DRAM on the EP's T2080. So the ATMU registers, LAWs, TLBs are set up correctly.

However, the test fails when using PCIe1. The configuration is exactly the same for all three controller setups. The SW simply is compiled to change the bus from PCIe4 to PCIe1 with appropriate memory changes to the controllers. We have a PCIe analyzer on the bus. We see the writes and reads complete as expected. But the data read back does not represent the data written in the prior step by the RC. When we break in with an emulator from the RC and examine the memory space mapped to the EP DRAM (BAR1) through the PCIe bus, it appears to be a repeating pattern. When I break in to the T2080 EP processor and examine DRAM it is unchanged from the original values written during DRAM init. What is different about PCIe1. I realize that PCIe1 supports SR-IOV, but I do not have that enabled.

0 Kudos
Reply
4 Replies

1,717 Views
scottgerhold
Contributor IV

I can provide the RC and EP dumps along with the LAW registers. Do you have a specific address range you want for the PCIe interface dumps? Any hidden registers you want (I know they exist as NXP has told us to change a couple in the past). Are you asking for both the normal registers and the PCIe configuration memory space (that is a little harder to get, but I can dump the screen from Lauterbach – which is 98% correct).

I am not sure what exactly you are asking for with the PEX analyzer dumps. If you are just looking for proof that what I said is true (that reads don’t return what was written, I can show that).

0 Kudos
Reply

1,675 Views
yipingwang
NXP TechSupport
NXP TechSupport

I can provide the RC and EP dumps along with the LAW registers. Do you have a specific address range you want for the PCIe interface dumps? Any hidden registers you want (I know they exist as NXP has told us to change a couple in the past). Are you asking for both the normal registers and the PCIe configuration memory space (that is a little harder to get, but I can dump the screen from Lauterbach – which is 98% correct).
[NXP] Yes. We want the dumps for the normal registers and the PCIe configuration space. Do this activity for both RC and EP. You may refer to Table 2-5. CCSR Block Base Address Map from T2080RM for PCIe offset. In addition, the register dump of LAW registers is also required.

I am not sure what exactly you are asking for with the PEX analyzer dumps. If you are just looking for proof that what I said is true (that reads don’t return what was written, I can show that).
[NXP] We need PEX analyzer dumps in the failing scenario, i.e., when reads don’t return the written data. It would be great if you also shared analyzer dumps in the passing case to compare.

0 Kudos
Reply

1,718 Views
scottgerhold
Contributor IV

I can provide the RC and EP dumps along with the LAW registers. Do you have a specific address range you want for the PCIe interface dumps? Any hidden registers you want (I know they exist as NXP has told us to change a couple in the past). Are you asking for both the normal registers and the PCIe configuration memory space (that is a little harder to get, but I can dump the screen from Lauterbach – which is 98% correct).

I am not sure what exactly you are asking for with the PEX analyzer dumps. If you are just looking for proof that what I said is true (that reads don’t return what was written, I can show that).

0 Kudos
Reply

1,738 Views
yipingwang
NXP TechSupport
NXP TechSupport
 
Please provide me the register dumps for PCIe interface, both RC and EP.
Provide the full console logs
PEX analyser dumps
 
Register dump of LAW registers is also required.
0 Kudos
Reply