T1042RDB CPLD RESET configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1042RDB CPLD RESET configuration

Jump to solution
1,022 Views
kurtehrhardt
Contributor II

On the T1042RDB, we believe our test equipment (Lauterbach debugger) to assert an HRESET_REQ when the SYSTEM.UP command is processed. If we first clear the DCFG_CCSR_CRSTSR1 (CCSR_BASE+E0400) by writing 1’s to it, subsequently we see its value is 0.  Then a SYSTEM.UP is performed.  Afterword, the DCFG_CCSR_CRSTSR1 reports a value of 0x1 (RST_PORST).  We are expecting a value of 0x2 (RST_HRESET).  This leads us to believe PORESET is being asserted to the T1042 not HRESET when the HRESET_REQ is made by the debugger.

The T1042RDB CPLD has a miscellaneous control and status register MISCCSR at address 0x17 from the base address of the CPLD. UBOOT maps the CPLD base address at 0xFFDF0000.  A memory dump of FFDF0017 shows a value of 0xB1.  The ‘B’ sets the REQ_MD bit field to ‘11’, which states “PORESET occurs when HRESET_REQ triggered”. We changed this value to 0x91, using UBOOT mw command, “HRESET occurs when HRESET_REQ triggered” and follow the above procedure. We still do not get the HRESET we are expecting.  In summary:

Sequence:

  1. Power cycle T1042RDB. Stop auto boot in UBOOT.
  2. Modify 0xFFDF0017 0x91. (Sets REQ_MD to ‘01’).
  3. Stop processor execution at the current instruction using breakpoint command in debugger.
  4. Clear DCFG_CCSR_CRSTSR1 to 0 by performing w1c on all bits (writing 0xFFFFFFFF) using debugger.
  5. Perform debugger “System.UP” (drives HRESET_REQ)
  6. Observe DCFG_CCSR_CRSTSR1 value (set to 1 (PORESET) not 2 (HRESET))

Is there a way to get the system behavior to act as expected (HRESET_REQ drives HRESET to T1042)? Do we need to reprogram the CPLD on the T1042RDB or is there some other method?

Regards,

Kurt Ehrhardt

Labels (1)
0 Kudos
Reply
1 Solution
646 Views
ufedor
NXP Employee
NXP Employee

> we believe our test equipment (Lauterbach debugger) to assert an

> HRESET_REQ when the SYSTEM.UP command is processed.

This assumption is not correct.

The T1024RDB JTAG connection is implemented in accordance with the AN4971 - QorIQ T1024 Family Design Checklist, Figure 23. JTAG interface connection - i.e. COP_HRESET_B is connected to the processor's PORESET_B.

View solution in original post

0 Kudos
Reply
1 Reply
647 Views
ufedor
NXP Employee
NXP Employee

> we believe our test equipment (Lauterbach debugger) to assert an

> HRESET_REQ when the SYSTEM.UP command is processed.

This assumption is not correct.

The T1024RDB JTAG connection is implemented in accordance with the AN4971 - QorIQ T1024 Family Design Checklist, Figure 23. JTAG interface connection - i.e. COP_HRESET_B is connected to the processor's PORESET_B.

0 Kudos
Reply